This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SYSCONFIG: Error: Cannot find module (copyutil.js)

Part Number: SYSCONFIG

Tool/software:

Posting on behalf of customer.

Issue is occuring when attempting to load the IS25LX046.json file.

Show Details provides the following:

Error: node:internal/modules/cjs/loader:1078

 

  throw err;

  ^

 

Error: Cannot find module 'C:\ti\ccs2020\ccs\eclipse\"C:\ti\mcu_plus_sdk_am261x_10_02_00_15\source\sysconfig\board\.meta\flash\copyutil.js"'

    at Module._resolveFilename (node:internal/modules/cjs/loader:1075:15)

    at Module._load (node:internal/modules/cjs/loader:920:27)

    at Function.executeUserEntryPoint [as runMain] (node:internal/modules/run_main:81:12)

    at node:internal/main/run_main_module:23:47 {

  code: 'MODULE_NOT_FOUND',

  requireStack: []

}

 

Node.js v18.16.0

 

    at window.eclipseSpawnCallback (http://localhost:63340/ccs-webview/sysconfig_PNGmOuHBh4y15abj/ui.js:312:773198)

    at http://localhost:63340/ccs-webview/sysconfig-shim.js:39:33

Best Regards,

Zackary Fleenor