Part Number: SYSCONFIG
Tool/software:
Posting on behalf of customer.
Issue is occuring when attempting to load the IS25LX046.json file.

Show Details provides the following:
Error: node:internal/modules/cjs/loader:1078
throw err;
^
Error: Cannot find module 'C:\ti\ccs2020\ccs\eclipse\"C:\ti\mcu_plus_sdk_am261x_10_02_00_15\source\sysconfig\board\.meta\flash\copyutil.js"'
at Module._resolveFilename (node:internal/modules/cjs/loader:1075:15)
at Module._load (node:internal/modules/cjs/loader:920:27)
at Function.executeUserEntryPoint [as runMain] (node:internal/modules/run_main:81:12)
at node:internal/main/run_main_module:23:47 {
code: 'MODULE_NOT_FOUND',
requireStack: []
}
Node.js v18.16.0
at window.eclipseSpawnCallback (http://localhost:63340/ccs-webview/sysconfig_PNGmOuHBh4y15abj/ui.js:312:773198)
at http://localhost:63340/ccs-webview/sysconfig-shim.js:39:33
Best Regards,
Zackary Fleenor