Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: EK-TM4C1294XL
Tool/software:
I'm using the EK-TM4C1294XL running a PTP (IEEE1588) slave clock to generate PPS signal on PG0 and comparing it with the PPS output from other two GNSS receivers from TRIMBLE and UBLOX.
Here how I'm initializing the EN0PPS:
MAP_GPIOPadConfigSet(GPIO_PORTG_BASE, GPIO_PIN_0, GPIO_STRENGTH_12MA, GPIO_PIN_TYPE_STD);
MAP_GPIODirModeSet(GPIO_PORTG_BASE, GPIO_PIN_0, GPIO_DIR_MODE_HW);
MAP_GPIOPinConfigure(GPIO_PG0_EN0PPS);
On my oscilloscope display, the falling edge of EN0PPS matches the rising edge of the other two GNSS receivers, but I can't understand or find any documentation explaining this.
I checked the GNSS receivers, and both have a PPS rising edge of TOS, which means the PPS rising edge matches exactly (too strong word) the beginning of the second.
Can someone please help me understand why the EN0PPS output is generating a falling edge on the beginning of the second?
Channel 1 on top is the EN0PPS and the other two the GNSS receivers PPS output.

Thanks,
Richard