Part Number: MCU-PLUS-SDK-AM243X
Other Parts Discussed in Thread: IND-COMMS-SDK
Tool/software:
We are also using IND-COMMS-SDK 9.2.0.24 and TMG PROFINET-Stack V6.0.0.0. Sending and receiving of telegrams works fine on port 1. Sending of telegrams seems also to work fine on port 2. But there is a problem with receiving of telegrams on port 2. When sending e.g. LLDP-telegrams from a device to DUT, ICSS_EMAC_rxInterruptHandler is called, but there is no frame in receive buffer of host port. By inspecting the L3 OCMC RAM I can see only fragments of the received frame at a wrong address in L3 OCMC RAM.