Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN, DP83640
Tool/software:
Hello,
I’m trying to get the HALCoGen EMAC_Loopback_TxRx example running on a TMS570LC43HDK. (Note: I also tried the lwIP example. Both fail at the same point.)
The MDIO module doesn’t seem to detect the PHY (DP83640): both MDIO_ALIVE and MDIO_LINK remain at 0x00000000. The program runs, but the PHY is never found.
My HALCoGen configuration:
I enabled only the EMAC-Driver.
Pinmux / IOMM
-
In Pin Muxing I enabled MII and the following signals:
-
RX:
MII_RXD[0] (P1),MII_RXD[1] (A14),MII_RXD[2] (G19),MII_RXD[3] (H18),MII_RXCLK (K19),MII_RX_DV (B11),MII_RX_ER (N19),MII_CRS (B4),MII_COL (F3) -
TX:
MII_TXD[0] (J18),MII_TXD[1] (J19),MII_TXD[2] (R2),MII_TXD[3] (E18),MII_TX_CLK (D19),MII_TXEN (H19) -
MDIO:
MDIO_D (G3),MDCLK (V5)
-
-
In Input Pin Muxing I switched these from Default Terminal to Alternate Terminal:
-
MDIO,MII_COL,MII_CRS,MII_RX_ER,MII_RXD[0..3],MII_TX_CLK
-
-
In Special Pin Muxing, MII is selected (not RMII).
Clocks / GCM
-
External clock source: 16.0 MHz (default).
-
PLL1 and PLL2 enabled at 300.00 MHz.
-
GCM mostly default:
VCLK3 = 75.0 MHz. I set VCLKA4 divider = 2, soVCLK4_DIV = 37.5 MHzandVCLKA4_S = 75.0 MHz.
EMAC / MDIO
-
In the EMAC tab I set the MAC address.
-
PHY address = 1, Channel = 0, Loopback enabled.
Board switches / LEDs
-
S2 switch set to Ethernet ON.
-
The PHY appears powered (green LED on the RJ45 is on).
I'm using the default code created by HALCoGen and the given example Code "example_EMAC_Loopback_TxRx.c" (unchanged) for the TMS570LC43x.
Does anyone have ideas what I’m missing or what I could try next to find out why MDIO never reports a live PHY?
Best regards,
Kilian