Other Parts Discussed in Thread: TMS570LS3137
Hello Support,
In the TRM spnu499.pdf, I see the following statement:
23.11 Interrupt Functionality
Interrupts can be generated on two interrupt lines:
1. DCAN0INT line
2. DCAN1INT line
These lines can be enabled by setting IE0 and IE1 bits respectively in CAN Control Register.
The DCAN provides three groups of interrupt sources: Message Object Interrupts, Status Change
Interrupts and Error Interrupts.( see
Figure 23-13 and Figure 23-14
)
In the TMS470LS3137 Datasheet I see there is a DCANx IF3 Interrupt Line.
How do I enable the above mentioned DCANx IF3 Interrupt Line on the DCANx Peripheral Side [similar to IE0 and IE1].
I am assuming DEx bits only affects the DMAREQ Lines from DCAN to DMA.
Also, in the TRM as shown in the above section, there is no mentioned of DCANx IF3 Interrupt Source.
Please help me understand the DCANx IF3 Interrupt Line better with more details.
Thank you.
Regards
Pashan