Part Number: LAUNCHXL2-570LC43
Other Parts Discussed in Thread: TMS570LC4357, HALCOGEN
Tool/software:
I am interfacing an SD card (SPI mode) to a TMS570LC4357 using MibSPI1 (I also tested MibSPI3 / SPI1 / SPI3). I have attached my project ZIP (Halcogen config + code). Below are my hardware connections and configuration — please let me know what else I should provide.
LaunchPad (TMS570LC4357) → SD Card Reader Module
SCLK (J5 Pin 7) → CLK
GOIA_0 (J4 Pin 10) → CS (I tried both GIOA_0 and MibSPI1_NCS_1)
SIMO_0 (J6 Pin 6) → MOSI / DI
SOMI_0 (J6 Pin 7) → MISO / DO
3.3V → VCC (I have also tested 5V on module)
GND → GND
I’ve attached my project files for reference. sd card interfacing with LAUNCHXL2-570LC43.zip
I am not getting any response from the SD Card (like 0x01 for idle state) which means SD Card Module has not interfaced yet.
What could be the possible reasons for this? Is there anything that i have missed?
Looking forward to your reply
Warm Regards
Radha Kishan Sharma