This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1290NCZAD: Writing using UART boot with Uniflash

Part Number: TM4C1290NCZAD
Other Parts Discussed in Thread: UNIFLASH

Hi experts,

Does Uniflash support writing via UART using the ROM boot loader for the TM4C series?(TM4C1290NCZADT3)

I can successfully write via UART using LM Flash Programmer. However, when using UART, the Verify feature is not available.
I am looking for a way to update the program using UART instead of JTAG and still be able to use the Verify function.

Best regards,
O.H