Part Number: AM2431
Other Parts Discussed in Thread: TPS65214, TPS65219
Hi experts,
Is there a PMIC available for the AM2431BSDFHIALVR with an MOQ of 500 or less (such as small T&R)?
The LP873345RHDT is considered unusable because buck0=0.75, and a VDD_CORE of 0.85 is required.
The large MOQ for the LP87334DRHDR and TPS65219x makes them difficult to select.
If it's difficult to answer here, offline communication is also acceptable.
Refer from: Using LP8733xx and TPS65218xx PMICs to Power AM64x and AM243x Sitara Processors
Best regards,
O.H