Part Number: AM2634
Other Parts Discussed in Thread: SYSCONFIG
Hi,
is the RAM initialisated after POR? Is that somewhere documentated?
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Nilabh,
what is the initialization value after PBIST of the RAM?
The RAM will be preserve after warm reset?
Regards, Holger
what is the initialization value after PBIST of the RAM?
For RAM bank0 and bank1, after PBIST, it will set to 0.
Even after warm reset RAM bank 0 and 1 will not be preserved
Hi Nilabh,
why is OCRAM only tested on partitions 0 and 1 and initialized by the BootROM? What about partitions 2 and 3?
Do these always have to be reset manually by the function SOC__rcmInitL2Memory as in the examples?
Customer assumes that partitions 2 and 3 have Mem Group ID (Number) 12 and 13.
He did not find a direct reference from L2OCRAM_BANKx_SLV to MEM_MSS_L2_x in the manual.

Regards, Holger
why is OCRAM only tested on partitions 0 and 1 and initialized by the BootROM? What about partitions 2 and 3?
It needs to be tested by SBL.
Do these always have to be reset manually by the function SOC__rcmInitL2Memory as in the examples?
Yes that is correct.
Customer assumes that partitions 2 and 3 have Mem Group ID (Number) 12 and 13.
He did not find a direct reference from L2OCRAM_BANKx_SLV to MEM_MSS_L2_x in the manual.
This can be found in Register addendum also.
Hi,
Why isn't all RAM tested?
Furthermore, can you interpret this in such a way that sections that are located in partitions 2 and 3 have absolutely no influence on the linker file initialization setting. Is that true?
For information, they are now checking the cause of reset on the POR to verify the data in this area. So they have a workaround for their problem.
So that they have a stable function in the future, they would like to know if there is a region in the entire memory where they can exchange data between the boot loader and the application program?
It is not in the sense of a shared section as they know it from the IPC. In their case, the programs do not run at the same time. One of the use cases for this area is the transmission of information from the application program to the bootloader before a software reset. In this case, saving to an external flash is not high enough.
Regards, Holger
Why isn't all RAM tested?
Thats by design, ROM performs PBIST on the region which it uses. If all regions are done boottime will be impacted.
Furthermore, can you interpret this in such a way that sections that are located in partitions 2 and 3 have absolutely no influence on the linker file initialization setting. Is that true?
I did not understand reasoning behind this, why would that be the case, If your SBL includes bank 2 and bank 3 and you have set initilization with 0 in your linker then they will be impacted, it depnds on how user creates linker.
So that they have a stable function in the future, they would like to know if there is a region in the entire memory where they can exchange data between the boot loader and the application program?
Ideally, this should be flash; if at all RAM is to be used, the application user has to design that paradigm.
It is not in the sense of a shared section as they know it from the IPC. In their case, the programs do not run at the same time. One of the use cases for this area is the transmission of information from the application program to the bootloader before a software reset. In this case, saving to an external flash is not high e
Again as stated before they would need to design and take care of it at application level.
Hello Nilabh,
so then you shouldn’t use partitions 2 and 3? And it is assumed that custom bootloader is never > 1MB?
So the ROM loader for the 2MB solution was never planned? Correct?
The configuration of the linker file is done using SysConfig. When they adjust the settings in SysConfig, there is no impact for partitions 2 and 3.
When executing this, he refers to the SOC__rcmInitL2Memory function. Is this correct?
Regards, Holger
So the ROM loader for the 2MB solution was never planned? Correct?
Yes, the max bootloader size is mentioned in TRM its less the 900MB
The configuration of the linker file is done using SysConfig. When they adjust the settings in SysConfig, there is no impact for partitions 2 and 3.
When executing this, he refers to the SOC__rcmInitL2Memory function. Is this correct?
These both are not related; the API does not depend on syscfg or linker utilized partitions.