Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM263P2-Q1: AM263P2 SPI Interface

Part Number: AM263P2-Q1
Other Parts Discussed in Thread: SYSCONFIG

Hi team,
      So  SPIx_D0 pin should be treated as MISO and Can i connect to the SPIx_D1 of the other MCU in an communication  between two MCU through SPI connection.

 

Regards

Jayakeerthana P

  • Hi Jayakeerthana,

    For SPI in Controller Mode:

    SPIx_D0 is MOSI by default and SPIx_D1 is MISO by default. However, these changes can be made within the SysConfig GUI - i.e. D0 can be configured as MISO and D1 can be configured as MOSI.

    D0 = MOSI (dpe0 = ENABLE)

    D1 = MISO (dpe1=DISABLE, inputSelect = 1)

    D0 = MISO (dpe0 = DISABLE)

    D1 = MOSI (dpe1 = ENABLE, inputSelect = 0)

    Alternatively, these settings can be modified for SPI Peripheral Mode by changing the 'mode' field in SysConfig.

    Regards,

    Brennan