This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM263P4-Q1: <ECP>PBIST error while accessing physical address

Part Number: AM263P4-Q1

Hello,

We are using PBIST example project from mcu_plus_sdk_am263px_11_00_00_19 to test the memories. Everytime when the content at 0x5330_0000 is viewed using memory browser after connecting to the target or during the debugging when "pInfo = &SDL_PBIST_InstInfoArray[instance];" of "SDL_PBIST_getInstInfo" function executes then we are continuously obsering below error as per the screen shot.


image.png

image.png

We have been seeing this behavior in AM263P CC boards. FYI, result is still the same after power cycle and system reset. 

Is there any method to enable PBIST physical memory to come out this issue?