Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: DMA possibilities to work with GPIO

Part Number: MSPM0G3507

Hello!

I found information that DMA can only write DOUTSET31_0 register and can't write or read any other.

But documentation actually says only "The GPIO peripheral allows the DMA write-access to the DOUT31_0 register".

There is no explicit information that other GPIO registers are restricted.

So where can I find explicit information about:

  1. Which memory regions are available for writing with DMA?
  2. Which memory regions are available for reading with DMA?

From forum: