This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Here is the English translation of your content:
My program uses mspm0_sdk_2_03_00_07 and KEIL tools, and I intend to use DMA Channel 1 together with TIMG6 to read data (digital signals) from a GPIO pin.
The DMA CH1 is configured as follows:
static const DL_DMA_Config gDMA_SAMPLE_READConfig = {
.transferMode = DL_DMA_SINGLE_TRANSFER_MODE,
.extendedMode = DL_DMA_NORMAL_MODE,
.destIncrement = DL_DMA_ADDR_INCREMENT,
.srcIncrement = DL_DMA_ADDR_UNCHANGED,
.destWidth = DL_DMA_WIDTH_WORD,
.srcWidth = DL_DMA_WIDTH_WORD,
.trigger = DMA_SAMPLE_READ_TRIGGER_SEL_FSUB_0,
.triggerType = DL_DMA_TRIGGER_TYPE_EXTERNAL,
};
static uint32_t sample_map[1024];
Afterward, my program sets parameters and starts the TIMG6 timer, and the source and destination addresses for the DMA are set as follows:
DL_DMA_setSrcAddr(DMA, DMA_SAMPLE_READ_CH, (uint32_t) &(SDA_GPIO_PORT->DIN31_0));
DL_DMA_setDestAddr(DMA, DMA_SAMPLE_READ_CH, (uint32_t) sample_map);
DL_DMA_setTransferSize(DMA, DMA_SAMPLE_READ_CH, 1024);
Then, the DMA is started and the program waits for it to complete:
DL_DMA_enableChannel(DMA, DMA_SAMPLE_READ_CH);
while (DL_DMA_isChannelEnabled(DMA, DMA_SAMPLE_READ_CH)) {
// waiting DMA completed
}
DL_TimerG_stopCounter(TIMER_SAMPLE_READ);
However, the result is that all elements in sample_map
are zero.
I had to use an SRAM variable as an intermediate buffer, and continuously update that variable with the value of SDA_GPIO_PORT->DIN31_0
in order for the DMA to correctly read pin data:
static uint32_t temp_data;
DL_DMA_setSrcAddr(DMA, DMA_SAMPLE_READ_CH, (uint32_t) &temp_data);
DL_DMA_enableChannel(DMA, DMA_SAMPLE_READ_CH);
while (DL_DMA_isChannelEnabled(DMA, DMA_SAMPLE_READ_CH)) {
temp_data = DL_GPIO_readPins(SDA_GPIO_PORT, SDA_1_GPIO_PIN | SDA_2_GPIO_PIN | SDA_3_GPIO_PIN | SDA_4_GPIO_PIN);
}
This way, the result is correct.
How do I setting and use DMA read GPIO PIN directly?
Hi,
Sorry form y mistake, it should be this:
DL_DMA_setDestAddr(DMA, DMA_SAMPLE_READ_CH, (uint32_t) &sample_map);
DMA need its 32bit address.
DL_DMA_setDestAddr(DMA, DMA_SAMPLE_READ_CH, (uint32_t) sample_map);
Regards,
Helic
I think the conclusion over here:
is that you can't.
Evidently the words [Ref TRM (SLAU846B) Sec 11.2.5] "The GPIO peripheral allows the DMA write-access to the DOUT31_0 register" mean Exactly what they say -- you can write to DOUT31_0 (but nowhere else) with the DMA, and you can't read any of the registers.