Part Number: MSPM0G3507
Hi All,
SYSPLL_ERR_01 includes a WA by FCC.
The clock accuracy of 5% does not refer to the accuracy of SysPLL itself. Rather, when using FCC, LFCLK (3%) and SYSOSC (1%) are utilized, so including the margin, 5% makes sense.
In other words, if you encounter a PLL that does not lock, you must use FCC, which results in an error of 5%.
If the PLL is functioning normally, FCC does not need to be used, so the clock accuracy depends on the clock source (for example, if SYSOSC and a normal PLL are used, it becomes 1%).
My understanding is that if you encounter a PLL that does not lock, you must restart the PLL until it locks. Is this correct?
Also, I have a question about the meaning of “does not lock.”
For example, if SYSOSC = 16 MHz and you multiply it by PLL to get 32 MHz, does “not locking” mean it stays at 16 MHz? Or does it mean the accuracy becomes worse? If the accuracy becomes worse, what level of accuracy should we expect?
Best Regards,
Ito