Part Number: MSPM0G3507
Other Parts Discussed in Thread: ADS131M08EVM, , , TIDA-010243
Hello,
We are attempting to build a Proof-of-Concept Prototype, based on the TIDA_010243 reference design, using the LP-MSPM0G3507 and ADS131M08EVM. The concept is to use the LP-MSPM0G3507 to capture data, via the SPI port, from eight (8) Wheatstone Bridges connected to the ADS131M08EVM: the connections made between boards are illustrated below.
LP-MSPM0G3507 ADS131M08EVM
(Controller) (Peripheral)
+-------------------------+ +-------------------------+
| | | |
| J1:1 +--( 3V3 )----------------------------+ DVDD (TP1) |
| | | |
| J3:21 +--( 5V )-----------------------------+ R70PAD (EVM_RAW_5V) |
| | | |
| J7 +--( PB27 - SYNC/RESET )-->-----------+ J10:1 (SYNC/RESET) |
| | | |
| J2:15 +--( PB8 - PICO )--------->-----------+ J10:2 (DIN) |
| | | |
| J2:24 +--( M0_CLKOUT )---------->-----------+ JP10: (8.192 MHz) |
| | | |
| J2:13 +--( PB6 – CS0 )---------->-----------+ J10:4 (CS) |
| | | |
| J1:7 +--( PB9 - SCLK )--------->-----------+ J10:5 (SCLK) |
| | | |
| J6 +--( PB26 - !DRDY )-------<-----------+ J10:6 (!DRDY) |
| | | |
| J2:14 +--( PB7 - POCI )---------<-----------+ J10:7 (DOUT) |
| | | |
| J2:20 +--( GND )----------------------------+ J10:8 (GND) |
| | | |
+-------------------------+ +-------------------------+
To view data using the existing "Energy-Metrology-GUI" [GUI] executable, extracted from ADCEnergyMetrologyLibrarySW_1.03:
1. Left the TIDA_010243 reference design code running on the LP-MSPM0G3507.
2. Exited Code Composer Studio [CCS].
3. Cycled power OFF then ON to both boards, to establish a clean, standalone startup and synchronization between boards.
4. Modified the .xml file, associated with the GUI executable file, to use one of the available COM ports (COM4, COM5, COM7, etc.).
5. Launched the GUI.
However, communication could not be established between the development PC and the LP-MSPM0G3507. Each of the three COM port numbers listed in "4." were used in the .xml file and attempted independently: each attempt failed.
Are there any adjustments (e.g.: code, .xml, hardware, etc.) that can be made to take advantage of the TIDA_010243 working design? If not, is there an alternate GUI I can use to view the data captured by the LP-MSPM0G3507? Please advise.
Thanks for your help.
Best,
Dag.FF2