This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0C1104: if there is an interrupt in the code and examples to determine if the UART bus is idle idle?

Part Number: MSPM0C1104

Hi Teams,

if there is an interrupt in the code and examples to determine if the UART bus is idle idle?

In addition, when the customer is using the development board, they suddenly cannot download the program, and the error message is as shown in the screenshot. Can you help me figure out how to solve this

Thank you!

image.png

  • Hi Vayne,

    There isn't an interrupt that says that the device is idle. However, there is a function that can be used to detect that. As for the issue you are seeing, most of the time it can be avoided if you restart CCS. However, if it was a hardware issue, could you share your schematics of your board to your local sales representative?

    Best Regards,

    Diego Abad