Part Number: MSPM0G3507
Other Parts Discussed in Thread: LP-XDS110ET, , UNIFLASH
Hey!
I have been working MSPM0 MCUs for a while now. For most part of my development I have used LP-MSPM0G3507. Now, I'm trying to use the XDS110-ET on an LP-MSPM0G3507 LaunchPad to program an external MSPM0G3507SRHBR chip following section 2.3.6 of the LaunchPad User's Guide.
Removed all J101 jumpers
Connected J102 SWDIO -> target SWDIO (PA20)
Connected J102 SWCLK -> target SWCLK (PA19)
Connected GND
Errors when attempting initial connection/programming:
CS_DAP_0: Error connecting to the target: DAP Connection Error. This could be caused by the device having gone to low power mode. Try forcing an external reset.If the error persists, try forcing BSL, a Mass erase or a Factory Reset. Check device FAQs for more information.
I'm trying to flash a new chip which has not been flashed before.
Is NRST connection mandatory ? My current hardware has NRST directly tied to VDD with no test point. I need to confirm if a hardware rework is necessary before proceeding.
Thank you.