Part Number: AM6442
Other Parts Discussed in Thread: SYSCONFIG
Hi, TI experts,
I'm implementing a warm reset booting from eMMC. However, after calling SOC_generateSwWarmResetMainDomain(), the eMMC fails to reset properly.
In my understanding, a normal reset should print the following messages to indicate a restart right after I call this function:
[BOOTLOADER_PROFILE] Boot Media : undefined
[BOOTLOADER_PROFILE] Boot Image Size : 175 KB
[BOOTLOADER_PROFILE] Cores present :
m4f0-0
r5f1-0
r5f1-1
a530-0
r5f0-0
r5f0-1
[BOOTLOADER PROFILE] SYSFW init : 12483us
[BOOTLOADER PROFILE] System_init : 5368613us
[BOOTLOADER PROFILE] Drivers_open : 39467us
[BOOTLOADER PROFILE] Board_driversOpen : 0us
[BOOTLOADER PROFILE] Sciclient Get Version : 9892us
[BOOTLOADER PROFILE] CPU Load : 2311966us
[BOOTLOADER_PROFILE] SBL Total Time Taken : 2373714us
Image loading done, switching to application ...
However, there is no print info. And I would like to ask if there are any other operations that need to be performed to complete the warm reset of EMMC booting.
Thanks,
xue.