This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2612: LP-AM261-PROC193A schematics,

Part Number: AM2612

Hello!

Can you please direct me to where from I can download the design files and schematics for LP-AM261-PROC193A ?

So far I was using LP-AM261-PROC193E2 and I was able to download the schematics for it from the link in the LP user manual, but the zip file contains only the files for PROC193E2 and PROC193E1, no files for PROC193A. 

The reason I need those is that now I have PROC193A as well on my desk and I want to check what are the needed changes that I have to apply in my SW to be compatible with it. I know the obvious differences (like the embedded PHYs, etc...) but I want to also verify the mapping of the rest of the IOs that I am using.

Thanks!