Part Number: AM2431
Hi,
The datasheet has been revised from REV G to REV H.
Regarding the section:
(Signal Descriptions - Power Supply): Updated the table notes associated with the CAP_VDDSx pins to clarify the need for capacitance derating and describe additional connectivity options .................................. 89
It states:
This pin must always be connected via a 6.3V or greater, 0.8uF to 1.5uF capacitor to VSS if the respectiVe VDDSHVx pin is eVer operated at 3.3V. The capacitor selected must proVide a capacitance within the defined range after it has been derated for DC bias.
My question is:
What happens if the capacitance is smaller than 0.8uF or larger than 1.5uF?
EVen when using capacitors with tolerance +-10% and temperature characteristic X7R (+-15%), the requirement cannot be satisfied without considering DC bias.
Example calculations:
1.0uF X7R, tolerance +-10% , temperature Variation +-15%
Max: 1.0 × (1.10 × 1.15) = 1.265uF
Min: 1.0 × (0.90 × 0.85) = 0.765uF
1.5uF X7R, tolerance +-10% , temperature Variation +-15%
Max: 1.5 × (1.10 × 1.15) = 1.897uF
Min: 1.5 × (0.90 × 0.85) = 1.147uF
Regards,
Futoshi