Part Number: MSPM0G1519
Similar to the two questions here:
and
I'm looking at powering an on board accelerometer which has a nominal current draw of 64uA with a GPIO pin. The purpose of powering this accelerometer from a GPIO pin directly is to minimize cost and complexity of adding another component, while maintaining the ability to perform a hard reset on the power to the device.
The 64uA shouldnt be an issue for the GPIO pin, however the on board accelerometer datasheet reccomends a 10uF capacitor on the power line.

The 10uF capacitor drives the inrush current well above the 6mA maximum for an SDIO pin.
Is this a concern for the uC pin that will cause damage?