Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357-EP: EMIF performance: max VLCK3 frequency for Async and sync mode?

Part Number: TMS570LC4357-EP

Team,
Can you please confirm which one of the below two posts is correct?

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/905741/tms570lc4357-emif-performance-for-sram
mentions that the max VCLK3 for both Sync and Async interface is 100Mhz

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/594509/tms570lc4357-emif-clock-for-asynchronous-access
mentions that max VCLK3 is 150Mhz for Sync interface and is 100Mhz for async interface.

What is the correct information?
Thanks in advance for confirming!

Anber

[EDITED] There might be some system level requirements that might limit the max EMIF_CLK that can be used.
For example the TRM document one of this use case:

 

  • Hi Anber,

    According to the datasheet EMIF section the min possible EMIF_CLK is mentioned as 10ns for synchronous operation that means max frequency should be 100Mhz only.

    The first forum post appears to be correct when stating that the maximum VCLK3 for both synchronous and asynchronous interfaces is 100 MHz, based on this timing specification.

    --
    Thanks & regards,
    Jagadish.