Part Number: TMDSCNCD263P
Other Parts Discussed in Thread: SYSCONFIG
Hi TI team,
I would like some clarification on the following points:
- Are 5 kHz, 10 kHz, and 20 kHz the only available excitation frequency options for the resolver angle/speed, or can we configure a variable excitation frequency? (image attached below)
- Can we feed the resolver ePWM output (RES0_PWMOUT0) into an external op amp amplifier as the excitation input signal?
- Does the RDC also accept single ended SIN and COS inputs instead of differential SIN+/SIN– and COS+/COS– signals?
- If excitation sine frequency at 10KHz, then I/P pwm frequency should be 320KHz, but it is observed about 800KHz at all frequencies (5K,10K and 20KHz)
Thanks & regards,
Shilpa