This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129XNCZAD: How to trigger an instant reset

Part Number: TM4C129XNCZAD

I still have the problem of a slow CPU on some boards, as described in this thread:

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1373456/tm4c129xnczad-help-when-i-power-up-my-device-without-the-jtag-cable-connected-the-display-becomes-sluggish/5246105#5246105

I have determined that if I just cause a CPU reset after the system is running, it comes up in "fast mode" with no latency or sluggish response.  Right now I'm doing it by putting it into an infinite loop and letting the watchdog reset the system.  Is there a way to trigger an instant reset, like by issuing a bad instruction?

Also, does the fact that a reset puts it in the right mode provide any new information that would help determine what the original issue is?

Thanks very much.

 

  • You can generate a system reset by setting APINT: SYSRESREQ=1. [Ref datasheet (SPMS444B) p. 183.]

    Driverlib provides the SysCtlReset() function to do this.

    From your description, my first guess would be something to do with crystal startup (maybe already oscillating?) or maybe power ramp.