This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2432: ACD Feature - CT21 Conformance

Part Number: AM2432

Hi everyone,

Starting from this thread that is locked now: https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1626568/am2432-am243x-ethernet-ip---acd-feature/6314872

I have tried with CT21 Conformance Tool on AM2432 LP as described in previous thread but I have obtained the same issue.

In the pictures below, you can see the error and the configuration of the switch. I have tried also with 100M - Full Duplex - Auto Neg OFF and with this setup. 

 

Switch1: 192.168.1.238

Switch2: 192.168.1.239

DUT: 192.168.1.10

PC: 192.168.1.1

 

Do you have any idea how to resolve?

         

  • Hi Stefano,

    based on my previous answer, have you considered the troubleshooting tip regarding using a dedicated test PC to run your test?

    Also, in your screen-shot I'm a bit confused about your switch configuration, are you setting up 1000M fixed speed? (1000M is not supported by the device!).

    Best regards,
    Pourya

  • Hi  Pourya,

    Yes, I have used another PC.

    This is the picture that shows that I have fixed 100M - FD. I have also used another Switch, but the result is the same.

  • Hi Stefano,

    As mentioned in the earlier E2E discussion, we cannot reproduce the issue on our side (the passing test results were also provided for your reference).
    If the problem is not within the stack itself and the hardware is the same (AM243x_LP), the problem must stem from the test configuration.
    Even if you want to test with latest tool (CT22), using the latest SDK (2026), the ACD test should succeed—except for the single, known failure in step 3.2.3, which is a bug in the CT22 tool , as has been confirmed by ODVA.

    I have already shared the recommended test‑setup troubleshooting tips, so I will not repeat them here.

    Best regards,
    Pourya
  • Ok, I will try with new SDK and CT22.

  • Hi Pourya,

    Also with CT22 and last SDK, I have the same issue with AM243x_LP. Now, I have bought your same managed switch.

    Best regards.

    Stefano

  • Hi Stefano,

    can you please confirm, did you use SDK 2026 with AM243x-LP, and ran ACD in CT22, correct?
    Could you please provide the test result and the Wireshark log?

    Best regards,
    Pourya

  • Hi Pourya,

    In the pictures below you can see what I am using.

    As attachment you can find Wireshark log and CT22 report.

     acd_report.zip

  • Hi Stefano,

    The problem appears to be that the MAC address in the target’s SOC file was not configured correctly.

    Your UART and Wireshark logs show that the device’s actual MAC address is 70:FF:76:1E:24:24, but when the CT22 attempts to create a conflict state it uses a different (incorrect) address. This discrepancy indicates that the SOC file was not updated with the proper MAC address. 

    For example:

    Which means, the CT22 is assuming another MAC address for your Target which I believe should be the root cause of the problems you see.
    Please update your SOC file accordingly and try again, specifically this sections:

    Best regards,
    Pourya