This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6422: SDK8.6 linux R5F1-0 ICSSG0

Part Number: AM6422

Hello,

    We are currently using SDK 8.6 and booting the real‑time cores under Linux. Now we want to use R5F1‑0 to drive the ICSSG0 Ethernet. After Linux boots, when we connect to R5F1‑0 using the emulator/debugger, it displays the following content. How can this problem be solved? 

 

[MAIN_Cortex_R5_1_0] 
Initializing all peripheral clocks
----------------------------------------------
Enabling clocks!

Opening all peripherals
----------------------------------------------

Initializing config EnetType:1, InstId :0
----------------------------------------------
Mdio_open: MDIO Manual_Mode enabled

icssg1-p1: Opening port 1
EnetPhy_bindDriver: PHY 4294967295: OUI:a7795f80 Model:7070707 Ver:a7777cf3 <-> 'generic' : OK

EnetUdma_initTxFreeDescQ: [Enet UDMA Error] Tx DMA descriptor memory allocation failed !!

EnetUdma_initTxFreeDescQ:
Assertion @ Line: 2002 in /nightlybuilds/mcupsdk_internal/jenkins/mcu_plus_sdk_am64x_09_02_01_05/source/networking/enet/core/src/dma/udma/enet_udma_priv.c: false