This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2432: AM2432 Power Estimate

Part Number: AM2432
Other Parts Discussed in Thread: TPS65219

Hi,

I am looking for the power consumption of the AM2432BSDGHIALXR processor so I can properly spec the power supply circuitry for it.

The datasheet links to the AM64x/AM243x Power Estimation Tool Application Note, and the app note has a link to a spreadsheet that seems to be dead: www.ti.com/.../SPRM779

Is there an updated link to the spreadsheet or another way I can download it? Thanks!

 

  • Hi,

    It is not recommended to use the Power Estimation Tool (PET) for supply sizing. PET can be used to estimate average active power and to input total SoC power into thermal simulations. For supply sizing, we recommend using regulators with electrical/thermal spec equivalent (or better) to the PMIC or discrete solution used in the SoC EVM. Alternatively, the maximum current ratings can also be used for supply sizing when designing custom power solution. Here are some reference documentation/tools.    

    Thanks,

    Brenda

  • Great, thanks for the resources and the advice on the power estimation. I'll design from the reference implementations and max current ratings. I appreciate the quick response!