Part Number: MSPM0L2228
Hi TI Team,
I am evaluating the Shutdown mode current consumption on the LP-MSPM0L2228 LaunchPad using the SDK example project sysctl_shutdown.syscfg. However, I am measuring a current consumption of approximately 3 mA in Shutdown mode, which is significantly higher than expected.
Here is my hardware setup for the current measurement:
-
Removed the 3V3 jumper in the J101 isolation block.
-
Connected an ammeter in series across the 3V3 jumper pins on J101.
Could you please review my setup and advise if I am missing any hardware/isolation steps or software configurations?
Specifically:
-
Are there any other jumpers on J101 (such as SWD/JTAG lines, UART, or backchannel XDS110 connections) that need to be removed to prevent back-powering or leakage current through the debug probe?
-
Are there any default onboard peripherals or pull-up/pull-down resistor paths on the LP-MSPM0L2228 that could contribute to this ~3 mA current draw in Shutdown mode?

Thanks and best regards,
Daniel