Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM263P4: AM263Px OTP eFuses and VPP operation

Part Number: AM263P4
Other Parts Discussed in Thread: LP-AM263P, UNIFLASH

Hi,

We are starting a new power-converter design based on AM263Px and would like to clarify the VPP supply requirements and software support for OTP eFuse programming.

According to the attached VPP_datasheet.pdf, VPP must be supplied at 1.7 V during programming, and no voltage should be applied to the VPP pin during power-up or normal operation. Could you confirm that this also applies when the eFuses are only being read?

The attached VPP_mr.pdf describes an alternative approach using the internal analog LDO, temporarily reducing its output from 1.8 V to 1.7 V during programming and restoring it afterward.

However, the attached EVK schematics show a permanent connection between VDDA18_LDO and VPP through a 0-ohm resistor:

  • PROC159B(001)_SCH.pdf: R467, sheet 13.

  • PROC171A.pdf: R189, sheet 5.

Could you clarify how this configuration complies with the datasheet requirement to leave VPP unpowered during normal operation? In particular, what is the role of VPP_EN_MMR.VPP_EN, and what should its state be before and after programming?

For our design, we would also appreciate your recommendation on whether to use an external 1.7 V supply or the internal analog LDO, including any restrictions on programming OTP eFuses in the field.

The datasheet instructs users to obtain the OTP programming software from their local TI representative. Could you confirm:

  • Which OTP Keywriter package is required for AM263Px, how to obtain it, and which MCU+ SDK and silicon revisions it supports.

  • Whether the package automatically handles the complete internal-LDO sequence, including voltage adjustment, reset masking, stabilization delays, verification, and restoration to normal operation.

  • Which host tools and communication interfaces are supported for loading and controlling the programming firmware.

  • Whether runtime OTP updates, such as incrementing anti-rollback revisions on an HS-SE device, use the same package or require TIFS-MCU services, and whether those services also manage the VPP/LDO sequence.

Best regards,

Andrea

  • Hi Andrea,

    This is a thorough set of questions. Addressing each area systematically.


    1. VPP During eFuse Reads vs. Programming

    Confirmed: The datasheet requirement applies to reads as well. During normal operation — including eFuse reads — the VPP pin must have no voltage applied (the spec lists it as "No Connection") 1. VPP is only required at 1.65–1.75 V (nominal 1.7 V) during active eFuse programming. eFuse contents are read from memory-mapped registers at boot without any VPP supply.


    2. EVK Permanent VDDA18_LDO-to-VPP Connection: Why It's Compliant

    The apparent conflict is resolved by understanding two facts:

    • There is no internal silicon connection between the VDDA18_LDO output pin and the VPP pin. The zero-ohm resistor on the EVK (R467/R189) creates an external PCB-level route 2.

    • Compliance is enforced in software, not hardware. The VPP_EN bit in the VPP_EN_MMR register acts as a gate. When VPP_EN = 0 (default), the internal path from the LDO to the eFuse array is disabled — even though 1.8 V is present on the VPP ball, it does not reach the fuse cells. Setting VPP_EN = 1 enables the supply path only during the programming window 3.

    The full software-controlled sequence before programming:

    1. Read TRIM_OFFSET from EFUSE_OVERRIDE_LDO_TRIM
    2. Assert MASK_ANA_ISO.MASK = 3b'111 (prevents LDO voltage change from triggering resets)
    3. Set LDO_PROG = 4b'1110 to lower the Analog LDO from 1.8 V → 1.7 V
    4. Restore TRIM_OFFSET to the value read in step 1
    5. Set OVERRIDE = 3b'111 to activate the voltage change
    6. Wait 1 ms for stabilization
    7. Set VPP_EN = 1
    8. Program and verify eFuses

    After programming, restoration is critical (device will malfunction if skipped):

    1. Clear OVERRIDE field → LDO returns to 1.8 V
    2. Wait 1 ms
    3. Clear MASK_ANA_ISO.MASK

    This procedure is documented in the AM263Px TRM Section 6.2.1.1 3 and also in the AM261 TRM 4.

    TI has confirmed this EVK configuration (VDDA18_LDO, VDDA18_OSC_PLL, and VDDA18 tied together and routed to VPP) is valid and reliable for mass production 5.


    3. External 1.7 V LDO vs. Internal Analog LDO — Recommendation

    Criterion Internal Analog LDO External 1.7 V LDO
    BOM cost / PCB area Lower — no extra component Higher — dedicated LDO needed (e.g., TLV75801PDRVR)
    Software complexity Requires the LDO reprogramming sequence above Simpler — just enable/disable the external supply
    Field programming Supported — VPP source is always on-board Supported if LDO is populated on-board
    Factory-only programming VPP source always present External supply can be kept off-board to save BOM
    Current capability VDDA18_LDO max output is 60 mA total (shared with VDDA18 pins) Can be sized to the 100 mA peak spec independently

    Recommendation: For a power-converter product where eFuse programming is typically a one-time factory operation, the internal Analog LDO approach (matching the LP-AM263P EVK reference design) is the preferred path — it eliminates an external component and is production-proven 6. Note the 60 mA LDO limit 7 vs. the 100 mA peak VPP spec — TI's EVK uses this configuration successfully, but if your design draws significant current from VDDA18 pins simultaneously during programming, consider the external LDO.

    If you need field programming capability, ensure the VPP path is present on-board (either the 0-ohm resistor to VDDA18_LDO, or a populated external LDO). Programming must occur at 0–50 °C ambient 1.


    4. OTP Keywriter Package

    Package name and access: The AM263Px OTP Keywriter (e.g., otp_keywriter_am263px_SR_10_11_01_01_00) is available free of charge under NDA from the TI restricted security portal: AM263PX-RESTRICTED-SECURITY 8. The silicon revision is encoded in the package name (SR_10 = Rev 1.0(A), etc.) — select the version matching your silicon 9. Known AM263Px silicon revisions are 1.0(A) and 1.2(C) 10.

    LDO sequence automation: Yes — the Keywriter software automatically handles the VDDA18_LDO voltage adjustment (1.8 V → 1.7 V), reset masking, stabilization delays, eFuse programming/verification, and restoration to 1.8 V 5. It also includes retry mechanisms and error correction (CRA single-bit, Row Replacement multi-bit) for hardware faults — though these are not a substitute for a stable VPP supply 11.

    Host tools and interfaces:
    - UART is the primary host interface, using the sbl_uart_uniflash binary (prebuilt in the MCU+ SDK, or rebuildable from source) 12.
    - OSPI boot is also documented as a supported boot path for the Keywriter 12.
    - JTAG (DevBoot mode) is noted as useful for JTAG-based Keywriter operations 3.
    - The package includes Linux and Windows installers 13.

    Package contents: HSM firmware (encrypted binary, not modifiable), SBL example (source, modifiable, SysConfig-enabled), TI-FEK public key, and certificate generation tools 13.


    5. Runtime Anti-Rollback Updates — Keywriter vs. TIFS-MCU

    These are two distinct mechanisms:

    OTP Keywriter TIFS-MCU HSM Client Services
    Purpose One-time device provisioning (HS-FS → HS-SE) Runtime security services on HS-SE devices
    Anti-rollback Can set initial SWRV values during provisioning Increments SWRV counters at runtime via HsmClient_writeSWRev()
    Who performs eFuse writes HSM ROM + Keywriter HSM FW TIFS-MCU (Cortex-M4F HSM Runtime)
    VPP required? Yes — 1.7 V on VPP pin Yes — all eFuse writes require 1.7 V on VPP 14

    Runtime anti-rollback flow: Embed a higher swrv value in the signed X.509 certificate, then call HsmClient_writeSWRev() from the application or bootloader. TIFS-MCU validates the signature and blows the thermometer-coded eFuse counter bits (32-bit for SBL SWRV, 32-bit for HSM SWRV, 64-bit for App SWRV) 15. R5F cores cannot directly write eFuse registers — hardware firewalls restrict access to TIFS-MCU only 15.

    Critical implication for field updates: Since runtime SWRV updates also require VPP = 1.7 V, your board must have the VPP supply path populated (internal LDO via 0-ohm resistor, or external LDO) if you plan to increment anti-rollback counters in the field. The TIFS-MCU HsmClient_writeSWRev() service handles the eFuse controller interaction, but the retrieved documentation does not explicitly confirm whether TIFS-MCU also automates the LDO voltage reprogramming sequence — this is a gap you should clarify with TI. An anti_rollback example is provided in the TIFS SDK for reference 15.

    Additional runtime OTP services available via HSM Client (HS-SE only): Read/Write/Lock OTP Row, Get OTP Row Count, Get OTP Row Protection, Read/Write SW Revision 16.

    Note: e-Fusing security keys permanently alters the device. TI disclaims all warranty liability for devices that have been e-Fused 1.


    Resources:

    1. AM263Px Datasheet — VPP Specifications
    2. E2E: AM263Px VPP Supply Clarification — Internal vs. External
    3. AM263Px TRM (SPRUJ55D) — eFuse Programming / LDO Override
    4. AM261 TRM — Section 6.2.1.1 Using the Device Analog LDO for VPP Supply
    5. E2E: AM263P4 eFuse Programming Configuration and Reset Behavior
    6. AM26x Hardware Design Guide — VPP Section
    7. E2E: VDDA18_LDO Current Capability
    8. E2E: HS-FS to HS-SE Migration — Keywriter and TIFS Add-On
    9. E2E: Building sbl_keywriter for AM263Px
    10. AM263Px Errata (SPRZ570E)
    11. E2E: Keywriter Issues — VPP Stability
    12. E2E: OTP Keywriter User Guide Questions
    13. AM26x Academy — OTP Keywriter
    14. AM26x Academy — Extended OTP
    15. E2E: AM263Px Deep Security Questions — Anti-Rollback
    16. MCU+ SDK AM263Px — HSM Client API Guide

    Best Regards,

    Zackary Fleenor