Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2612-Q1: OSPI booting upon power on

Part Number: AM2612-Q1
Other Parts Discussed in Thread: UNIFLASH

We have used AM2612ALDFHMZCZRQ1 controller which is ZCZ package. Please guide us how to implement booting from OSPI upon power without a debugger or UART connection.
Currently I have isolated GPIO 61 from OSPI flash. Power on reset working normal upon power on.

We have kept boot switch in oSPI mode.

Boot from flash.pdf 

  • Hi Vignesh, 

    Please follow the below steps mentioned in the FAQ

     [FAQ] AM263P4-Q1: How to flash/program custom external flashes 

    Post this, build the SBL, examples/drivers/boot/sbl_ospi_multicore_elf and upload this in Uniflash at 0x6000_0000 address in flash. Please note that the SBL should have the same flash and ospi configurations based on the FAQ 'How to flash/program custom external flashes'.

    Build the application and upload it in UniFlash at the address 0x6008_1000. 

    Now load the image, put device in OSPI boot mode and POR. 

    You should be able to see ROM boot the SBL and SBL boot the application.

    Thanks & Regards,

    Aswin

  • Hi Aswin 
      

         I have tried below mentioned instruction we are not able boot flash. When are able read data from memory and write data to memory via OSPI in Dev boot mode. Controller is not able boot from OSPI in OSPI boot mode. Please provide us suitable solution.

  • Hi, 

    - I assume you are able to run ospi flash io example and have configured the Flash/OSPI configuration of SBL and Flasher accordingly.

    - In OSPI boot mode, when powering on, what is the message that is coming in UART? Any CCC logs is coming?

    - Can you tell me the value of this register: 5320 010Ch. You can take this connecting the debugger and entering this address in the memory browser.

    - Also can you take the flash memory dump and ensure that the flashed images are reflected in the memory.

    Thanks &  Regards,

    Aswin