AM2612: AM2612 PROFINET – Custom Stack Configuration

Part Number: AM2612

I have updated my previous post to correct some incorrect information. I apologize for any confusion.

Hello TI Support Team,

We are developing a modular PROFINET IO Device based on the AM2612 using Industrial Communications SDK 2026.00.00.06.

Our product is a modular remote I/O device that communicates with an external PROFINET IO Controller (PLC). We are not developing an IO Controller.

1. Target Requirements

Our target system has the following requirements:

  • PROFINET IO Device functionality

  • 1 DAP slot (Slot 0)

  • Up to 32 expansion I/O module slots (Slots 1–32)

  • Dynamic module/submodule plug and pull

  • PROFINET RT and IRT support

  • MRP (Media Redundancy Protocol) support

  • Two Ethernet ports (ICSSM0, MII interface)

  • Support for a standard single IO-Controller connection

  • Up to 1,440 bytes of process data, with input and output limits to be confirmed

2. Current PROFINET Stack Configuration

The current PROFINET stack configuration includes the following macros:

#define PN_API_IOD_MAX_NUM_OF_SLOTS              9
#define PN_API_IOD_MAX_NUM_OF_SUBSLOTS_PER_SLOT   10
#define PN_API_IOD_NUM_OF_IO_AR                   4

According to the TI documentation, these macros should not be modified directly because the precompiled PROFINET stack library was built using these settings.

We also noticed that the documentation mentions the possibility of extending the number of subslots upon customer request.

3. Questions

Q1. Maximum Slot Configuration

Our application requires 33 slots, including the DAP at Slot 0 and 32 expansion I/O slots.

  • Does PN_API_IOD_MAX_NUM_OF_SLOTS include the DAP slot?

  • Can the existing PROFINET IO Device stack support 33 slots through application-level configuration?

  • If not, is a custom-built stack library required?

Q2. Custom PROFINET Stack Library

If the current precompiled library does not support 33 slots:

  • Can TI provide a customized PROFINET IO Device stack library supporting at least 33 slots?

  • Is there an officially supported method to configure these compile-time limits?

  • Would such a customized library retain full RT, IRT, and MRP support?

Q3. Subslot Configuration

  • What is the maximum total number of subslots supported by the current library?

  • Can the number of subslots be increased independently of the slot count?

  • Is a custom library required to extend the slot and subslot limits?

Q4. Process Data Size

Our target process data size is up to 1,440 bytes.

  • What are the maximum input and output process data sizes supported by the current IO Device stack?

  • Can the maximum process data size be increased for a single IO-Controller connection?

  • Are there different process data limitations when operating in RT versus IRT mode?

  • Would increasing the process data limits require rebuilding the stack library?

Q5. IRT and MRP Support

We intend to support both PROFINET IRT and MRP.

  • Can IRT and MRP be supported together with a 33-slot configuration?

  • Are there any specific limitations or resource requirements for this combination?

  • Would extending the slot/subslot configuration affect IRT cycle-time performance or MRP functionality?

Q6. AR Configuration

Our device will normally communicate with a single IO Controller.

The current stack is configured with:

#define PN_API_IOD_NUM_OF_IO_AR 4
  • Can we retain the default configuration even when only one IO Controller is connected?

  • Is it possible to reduce the maximum number of IO ARs to optimize RAM usage?

  • Would this require a customized stack library?

Q7. Dynamic Module Handling

  • Can the existing PN_API_IOD_plugSubmod() and PN_API_IOD_pullSubmod() APIs support dynamic module replacement across all 32 expansion slots?

  • Are there any additional restrictions on module plug/pull behavior during RT or IRT operation?

  • Does the stack support the corresponding PROFINET diagnosis and alarm handling?

Q8. Memory Requirements and Support

If a customized PROFINET stack library is necessary:

  • What would be the expected additional Flash and RAM requirements?

  • Can TI provide a precompiled library with the requested configuration?

  • Would this require Premium support or a separate licensing agreement?

  • Would the customized library affect PROFINET conformance testing or certification?

4. Summary

Our primary goal is to implement a modular PROFINET IO Device with 33 slots while retaining RT, IRT, and MRP functionality.

We would like to determine whether this can be achieved using the existing AM2612 PROFINET stack library or whether TI needs to provide a customized library with extended slot, subslot, and process data limits.

We would appreciate your guidance on the supported configuration options and recommended implementation approach.

Best regards.