Part Number: AM2612
Hello TI Support Team,
We are developing a PROFINET IO-Device using the AM2612 and the Industrial Communications SDK ind_comms_sdk_am261x_2026_00_00_06 with PROFINET Device stack version 4.4.0.
Our internal communication test has completed. Slots 1 through 4 work correctly, but the device does not recognize or exchange process data for Slot 5 and above, up to Slot 32. We also changed the related configuration macros in the application source and rebuilt the application, but the behavior did not change.
The attached GSDML allows modules to be configured in Slots 1 through 32. Each module definition currently contains one virtual submodule.
Could you please confirm:
- What is the maximum slot count supported by the AM261x PROFINET Device 4.4.0 stack library included in this SDK?
- Is the slot limit compiled into the prebuilt stack library, such that changing application macros alone cannot increase it?
- Can TI provide or generate a custom stack library supporting at least 32 slots for AM2612?
- Does this customization require the TI Custom Offer subscription, and is it part of the Premium package or a separate commercial offering?
- What information, license, and estimated lead time are required to obtain the custom library?
- Are there additional limitations related to subslots per slot, total subslots per AR, process-data size, number of ARs, or cycle time for this configuration?
We can provide the GSDML, application configuration, build details, and test logs for further analysis. Since the customer is also evaluating EtherCAT and Ethernet communication on this device, an early clarification of the PROFINET customization path would be appreciated.
Best regards,
Jack Cha