TMS320C40: C Compiler for TMS320C4X

Part Number: TMS320C40

Hello,

We are trying to revive an old build setup that uses a TMS320C40. 
I need to get in contact with the local FAE for the New Hampshire, USA region so that the appropriate support can be provided.
Any help is greatly appreciated.

  • Hello Henry,

    Please keep in mind that TMS320C40 is an extremely old part. We're talking older than many of our team members, old enough that docs and software got sent through the mail instead of the internet. We can point you to the Code Composer tool if your company purchased a license back in the day, and the compiler, but we won't be able to offer any design support or answer any questions about the hardware or software.

    If that's all you need, I will send you over to the CCS / compiler team to continue the conversation.

    If you would want design support, I would recommend evaluating a more recent part. I could connect you with either our marketing team or your company's TI representative as needed to discuss more recent devices.

    More details - AI summary 

    AI generated info, but looks good:

    Reviving the build setup

    Toolchain you need (not modern CCS): the C40 predates Code Composer Studio entirely. You need the older non-Eclipse "Code Composer" v4.10 (plus up to 2 service packs) and the separate C3x/C4x compiler — reported versions 4.6–4.7 5. A single floating-point compiler/assembler/linker set covers C30, C31, and C40 6, and the tools use COFF object format 7.

    Common pitfall: installing only a service pack patch fails unless the base product "Code Composer 4.10 'C3x-C4x'" is already present — TI's CCS support team handles these escalations when the files aren't on the public product page 8.

    If you still have a working machine: for command-line (non-IDE) use, the legacy toolchain can often be copied file-by-file to a new machine — run under BASH or DOSBOX — avoiding the installer and its registry changes. TI support confirmed this as viable 3.

    Debug side: legacy C40 setups used an XDS510 or SP1510/525 JTAG probe (often parallel-port) with EMU4XW.EXE as the command-line debugger, documented in the TMS320C4x C Source Debugger User's Guide 1. Parallel-port hardware is the usual blocker on modern PCs.

    Reference manuals: TMS320 Floating-Point DSP Assembly Language Tools User's Guide (SPRU035) and Optimizing C Compiler User's Guide (SPRU034) cover C3x/C4x build and link flow 9.

    Gap to flag: the C4x compiler installers are not available from any current TI download page — they exist only through the support-representative route above. Tell us your host OS, existing compiler version, and JTAG hardware, and the request can be scoped precisely.

    Follow up: Which compiler version and JTAG probe does your existing setup use, and are you targeting a command-line rebuild or the full Code Composer 4.10 IDE?

    1. E2E: TMS320C40 Code Composer for TMS320C40
    2. TMS320C6678 product page
    3. E2E: Need old version of CCS for TMS34020
    4. E2E: Code Composer 4.10 download
    5. E2E: TMS320C40 environment building
    6. SPRU083
    7. SPRU035D
    8. E2E: Compiler TMS320C40
    9. SPRU084A