Other Parts Discussed in Thread: LM3S5632, LM3S3748, TM4C123GH6PGE
customer said:With the possible migration from LM3S5632 to LM4F131E5QR, I am wondering if it is transparent for the Stellaris library, which the firmware application is based on.
I have developed some code based on the LM3S3748 EVK
In your case, this migration can be described in A number of ways:
LM3S5632 to LM4F131E5QR
DustDevil Class to Blizzard Class
LM3S to LM4F
Stellaris ARM Cortex-M3 to Stellaris ARM Cortex-M4
From top to bottom shows the the most specific to the most general description. For example, every DustDevil class device is a LM3S device. However, not every LM3S device is a DustDevil device.
TI makes StellarisWare so that it’s easy to move software among the Stellaris classes. StellarisWare is made of three parts:
1. Stellaris® USB Library
C:\StellarisWare\docs\SW-USBL-UG-8555.pdf
2. Stellaris® Peripheral Driver Library
C:\StellarisWare\docs\SW-DRL-UG-8555.pdf
3. Stellaris® Graphics Library
C:\StellarisWare\docs\SW-GRL-UG-8555.pdf
The Driver Library includes drivers for all classes of Stellaris microcontrollers. Some drivers and parameters are only valid for certain classes. See the application report entitled, "Differences Among Stellaris Product Classes" for more information. The LM3S5632 is a DustDevil class device. The LM4F131E5QR is a Blizzard class device.