Hi,
I've run into a problem creating the CMSIS dsplib library. I am using the stellaris launchpad. I have successfully run programs on the launchpad and want to use the floating point dsp functions in the CMSIS library.
I followed the instructions in document SPMA041B "Using the CMSIS DSP Library in Code Composer Studio for Stellaris" but when it came to section 3.4 Editing the dsplib project settings, I don't see any reference in my properties to a TMS470 compiler. I see an ARM compiler. All of the compiler/linker property options mentioned in the document could be set for the ARM compiler and so I pressed on. but when it came to building the project I got a "can't open cmsis_ccs.h" error. I can't see a cmsis_ccs.h file anywhere. What am I doing wrong?
Regards,
Donald