Part Number: EK-TM4C123GXL
Other Parts Discussed in Thread: TM4C123GH6PM
Hello,
I think I have successfully compiled the DSPLibrary in CCS 6.2 to use with the Tiva C TM4C123GH6PM. I did the procedure exactly like described in the doc "Using the CMSIS DSP Library in Code Composer Studio for TM4C MCUs" - spma041g.pdf
Just in step 6 on page 9 I cant select the "Use unified assembly language (--ual)" checkbox. I never found this option in the properties. Could this be a problem?
Out of the ARM example folder I ran the complex floating point example without any error. If I use the integer real fft to save resources the code jumps into FaultISR while executing line "arm_rfft_q15(.....".
#include "arm_math.h"
#include "arm_const_structs.h"
#define TEST_LENGTH_SAMPLES 1024
extern uint16_t ui16InputTestData[TEST_LENGTH_SAMPLES];
static uint16_t ui16TestOutput[TEST_LENGTH_SAMPLES];
/* ------------------------------------------------------------------
* Global variables for FFT Bin Example
* ------------------------------------------------------------------- */
uint32_t fftSize = 1024;
uint32_t ifftFlag = 0; /* forward fft*/
uint32_t doBitReverse = 1; /* output NOT in bitreversal*/
/* Reference index at which max energy of bin ocuurs */
uint32_t refIndex = 213, testIndex = 0;
/* ----------------------------------------------------------------------
* Max magnitude FFT Bin test
* ------------------------------------------------------------------- */
int32_t main(void) {
arm_rfft_instance_q15 fft_ins;
// REAL integer FFT
arm_rfft_init_q15(&fft_ins, fftSize, ifftFlag, doBitReverse);
arm_rfft_q15(&fft_ins, (q15_t *) ui16InputTestData,
(q15_t *) ui16TestOutput);
while (1)
; /* main function does not return */
}
/** \endlink */
What did I wrong?
Thanks for any suggestions.