This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1) LM4F120H5QR ROM USER'S GUIDE ROM-LM4F120H5QR-UG-730 suggests to define TARGET_IS_BLIZZARD_RA1, which causes the rom.h from TivaWare 1.0 NOT to export any EEPROM API functions.
2) Tiva" TM4C1233H6PM ROM USER’S GUIDE ROM-TM4C1233H6PM-UG-750 suggests to define TARGET_IS_BLIZZARD_RB1, which causes the rom.h from TivaWare 1.0 to export EEPROM API functions. However, the TM4C1233H6PM ROM user''s guide doesn't document any EEPROM functions.
(where the TM4C1233H6PM should be identical to the LM4F120H5QR)
3) Looking in the ROM table for an example LM4F120H5QR Rev A3 shows EEPROM functions and:
- Calling ROM_EEPROMSizeGet returns the expected value of 2048.
- Calling ROM_EEPROMBlockCountGet returns the expected value of 32.
My questions are:
a) When compiling for a LM4F120H5QR should TARGET_IS_BLIZZARD_RA1 or TARGET_IS_BLIZZARD_RB1 be defined?
b) Should the ROM EEPROM functions be described as supported in the LM4F120H5QR and/or TM4C1233H6PM ROM user guides?
The ROM users guides didn't make it clear the significance of the suffix for the TARGET_IS_BLIZZARD macros. The "Using the ROM" section of the TivaWare™ Peripheral Driver Library USER’S GUIDE SW-DRL-UG-1.0 clarifies that the suffix represents the silicon revision targetted. i.e. for a LM4F120H5QR rev A3 this means TARGET_IS_BLIZZARD_RA3 should be defined.Chester Gillon said:When compiling for a LM4F120H5QR should TARGET_IS_BLIZZARD_RA1 or TARGET_IS_BLIZZARD_RB1 be defined?
However, the TivaWare 1.0 user's guide doesn't appear to have an up to date list of the defines expected by driverlib/rom.h since section 29.2 lists the following macros:
- TARGET_IS_DUSTDEVIL_RA0
- TARGET_IS_TEMPEST_RB1
- TARGET_IS_TEMPEST_RC1
- TARGET_IS_TEMPEST_RC3
- TARGET_IS_TEMPEST_RC5
- TARGET_IS_FIRESTORM_RA2
- TARGET_IS_BLIZZARD_RA1
Whereas the list of defines expected by the TivaWare 1.0 driverlib/rom.h are actually:
- TARGET_IS_BLIZZARD_RA1
- TARGET_IS_BLIZZARD_RA3
- TARGET_IS_BLIZZARD_RB1
For the TM4C123GH6PGE MCU, which Blizzard class should be designated? And where is this list? All previously listed links are BROKEN!!!
Hello Evelyn,
When using TM4C123 or LM4F please check the SYSCTL.DID0 register at address 0x400FE000
This is mentioned in the Data Sheet as well for the description of the above register.
If the value shows 0x18050001: The last byte which shows 01 and byte before it shows 00 means RA1
If the value shows 0x18050101: The last byte which shows 01 and byte before it shows 01 means RB1
Regards
Amit
Robert Adsett said:Someone from xyz should have an answer.
If they don't - may we drive a stake thru this Franken-post?
Sounds (exactly) like (another) day in Margaritaville...
Recall - we exhausted the torches - last "eclipse viewing..." I've several hundred "Stellaris match books" left over (they had "flash" issues) - might they do?
And while poster Robert, "Seizes this particular moment/issue" does not this, "Unclear locating" (to be kind) of, "Vital Tech Data" extend far beyond this focused request?
Many note the pristine, unmissable, RED BAR - spanning the forum's top - reserved for the "uber-important" blogs, groups videos - yet there is ...NO SPACE for, "Vital Tech Data!"
How can this possibly be justified?
Section 34.2 Direct ROM Calls of the TivaWareTM Peripheral Driver Library USER’S GUIDE SW-TM4C-DRL-UG-2.1.2.111 has a description of the TARGET_IS_* macros. Does that answer your question?Joseph Forrest said:I tried searching the user guide for the tm4c123gh6pm, the tm4c123x rom users guide, and the tivaware peripheral driver library users guide for an explanation but didn't find anything.
The latest TivaTM C Series TM4C123x ROM USER’S GUIDE UG-ROM-TM4C123x-818 SPMU367 dated May 2014 still doesn't contain mention of EEPROM functions, so I submitted documentation feedback.Chester Gillon said:b) Should the ROM EEPROM functions be described as supported in the LM4F120H5QR and/or TM4C1233H6PM ROM user guides?
[Whereas the TivaTM C Series TM4C129x ROM USER’S GUIDE UG-ROM-TM4C129x-818 SPMU363 does document the EEPROM functions]