This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ROM_UpdateUART() problem



Hi,

I'm having trouble with the ROM bootloader. I'm using an LM4F Launchpad.

If I put these lines as the first lines of my Main() ...

ROM_SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ); //set the clocking to run from the PLL at 50MHz
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
ROM_UARTConfigSetExpClk(UART0_BASE, ROM_SysCtlClockGet(), 38400, (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));

ROM_UpdateUART(); //will not return from here - needs hardware reset

...the ROM_BootLoader is run and I can update the code using LMFlash with AutoBaud Off fixed at 38400. All good as a test and is equivalent to the example that Chester found for me yesterday.

Now I want to be able to run the bootloader from within my app (which uses the UART with interrupt driven fifos), so I use this code...

ROM_IntMasterDisable(); //disable interrupts
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_GPIOA); //get UART reset to simple, no interrupts, no handshake
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_UART0);

ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
ROM_UARTConfigSetExpClk(UART0_BASE, ROM_SysCtlClockGet(), 38400, (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));

ROM_UpdateUART(); //will not return from here - needs hardware reset

...this appears to run the bootloader but I cannot get LMFlash to communicate.

Suspecting that there's something left running in my code which is interfering with the proper operation of the bootloader I tried a software reset...

...so from within my app I call ROM_SysCtlReset()

then at the top of my Main() I have...

if((ROM_SysCtlResetCauseGet() & SYSCTL_CAUSE_SW) != 0) {   //detect if reset came from within app
 ROM_SysCtlResetCauseClear(SYSCTL_CAUSE_SW);

 ROM_SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ); // Set the clocking to run from the PLL at 50MHz
 ROM_IntMasterDisable(); //disable interrupts master
 ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
 ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
 ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
 ROM_UARTConfigSetExpClk(UART0_BASE, ROM_SysCtlClockGet(), 38400, (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));

 while(ROM_UARTCharsAvail(UART0_BASE)) //empty the fifo just incase?
  i = ROM_UARTCharGetNonBlocking(UART0_BASE);

 ROM_UpdateUART(); //will not return from here - needs hardware reset

}

...but I still cannot get LMFlash to communicate

Can anyone suggest what I've done wrong please?

Thank you.

  • I found a few extra bytes being sent to the uart from my test console after I had entered the bootloader. The bootloader protocol is not robust against this sort of abuse. To who ever is updating the documentation please add "you should ensure all uart traffic has completely stopped before entering the bootloader" - obvious really - sorry for being an idiot :(