Other Parts Discussed in Thread: HALCOGEN, RM48L952
Hi Anthony,
I got a strange problem. I want use GIOB[2] as a input. But I can not got the value of this pin.
For GIOB[2], I have gated off the Emif_CLK in HCG(HALCoGen 03.05.02). I changed the level of the pin through hardware and read the value by the code showed below, but it did not change. Because this is a specific, I maybe make some mistakes.
Would you help me to find the problem.
void gioInit(void)
{
/* USER CODE BEGIN (2) */
/* USER CODE END */
/** bring GIO module out of reset */
gioREG->GCR0 = 1U;
gioREG->INTENACLR = 0xFFU;
gioREG->LVLCLR = 0xFFU;
/** @b initialize @b Port @b A */
/** - Port A output values */
gioPORTA->DOUT = 0U /* Bit 0 */
| (0U << 1U) /* Bit 1 */
| (0U << 2U) /* Bit 2 */
| (0U << 3U) /* Bit 3 */
| (0U << 4U) /* Bit 4 */
| (0U << 5U) /* Bit 5 */
| (0U << 6U) /* Bit 6 */
| (0U << 7U); /* Bit 7 */
/** - Port A direction */
gioPORTA->DIR = 0U /* Bit 0 */
| (0U << 1U) /* Bit 1 */
| (0U << 2U) /* Bit 2 */
| (0U << 3U) /* Bit 3 */
| (0U << 4U) /* Bit 4 */
| (0U << 5U) /* Bit 5 */
| (0U << 6U) /* Bit 6 */
| (0U << 7U); /* Bit 7 */
/** - Port A open drain enable */
gioPORTA->PDR = 0U /* Bit 0 */
| (0U << 1U) /* Bit 1 */
| (0U << 2U) /* Bit 2 */
| (0U << 3U) /* Bit 3 */
| (0U << 4U) /* Bit 4 */
| (0U << 5U) /* Bit 5 */
| (0U << 6U) /* Bit 6 */
| (0U << 7U); /* Bit 7 */
/** - Port A pullup / pulldown selection */
gioPORTA->PSL = 0U /* Bit 0 */
| (0U << 1U) /* Bit 1 */
| (0U << 2U) /* Bit 2 */
| (0U << 3U) /* Bit 3 */
| (0U << 4U) /* Bit 4 */
| (1U << 5U) /* Bit 5 */
| (0U << 6U) /* Bit 6 */
| (0U << 7U); /* Bit 7 */
/** - Port A pullup / pulldown enable*/
gioPORTA->PULDIS = 0U /* Bit 0 */
| (0U << 1U) /* Bit 1 */
| (0U << 2U) /* Bit 2 */
| (0U << 3U) /* Bit 3 */
| (0U << 4U) /* Bit 4 */
| (1U << 5U) /* Bit 5 */
| (0U << 6U) /* Bit 6 */
| (0U << 7U); /* Bit 7 */
/** @b initialize @b Port @b B */
/** - Port B output values */
gioPORTB->DOUT = 0U /* Bit 0 */
| (0U << 1U) /* Bit 1 */
| (0U << 2U) /* Bit 2 */
| (0U << 3U) /* Bit 3 */
| (0U << 4U) /* Bit 4 */
| (0U << 5U) /* Bit 5 */
| (0U << 6U) /* Bit 6 */
| (0U << 7U); /* Bit 7 */
/** - Port B direction */
gioPORTB->DIR = 0U /* Bit 0 */
| (0U << 1U) /* Bit 1 */
| (0U << 2U) /* Bit 2 */
| (0U << 3U) /* Bit 3 */
| (0U << 4U) /* Bit 4 */
| (0U << 5U) /* Bit 5 */
| (0U << 6U) /* Bit 6 */
| (0U << 7U); /* Bit 7 */
/** - Port B open drain enable */
gioPORTB->PDR = 0U /* Bit 0 */
| (0U << 1U) /* Bit 1 */
| (0U << 2U) /* Bit 2 */
| (0U << 3U) /* Bit 3 */
| (0U << 4U) /* Bit 4 */
| (0U << 5U) /* Bit 5 */
| (0U << 6U) /* Bit 6 */
| (0U << 7U); /* Bit 7 */
/** - Port B pullup / pulldown selection */
gioPORTB->PSL = 0U /* Bit 0 */
| (0U << 1U) /* Bit 1 */
| (1U << 2U) /* Bit 2 */
| (0U << 3U) /* Bit 3 */
| (0U << 4U) /* Bit 4 */
| (0U << 5U) /* Bit 5 */
| (0U << 6U) /* Bit 6 */
| (0U << 7U); /* Bit 7 */
/** - Port B pullup / pulldown enable*/
gioPORTB->PULDIS = 0U /* Bit 0 */
| (0U << 1U) /* Bit 1 */
| (0U << 2U) /* Bit 2 */
| (0U << 3U) /* Bit 3 */
| (0U << 4U) /* Bit 4 */
| (0U << 5U) /* Bit 5 */
| (0U << 6U) /* Bit 6 */
| (0U << 7U); /* Bit 7 */
/* USER CODE BEGIN (3) */
/* USER CODE END */
/** @b initialize @b interrupts */
/** - interrupt polarity */
gioREG->POL = 0U /* Bit 0 */
| (0U << 1U) /* Bit 1 */
| (0U << 2U) /* Bit 2 */
| (0U << 3U) /* Bit 3 */
| (0U << 4U) /* Bit 4 */
| (1U << 5U) /* Bit 5 */
| (0U << 6U) /* Bit 6 */
| (0U << 7U) /* Bit 7 */
| (0U << 8U) /* Bit 8 */
| (0U << 9U) /* Bit 9 */
| (1U << 10U)/* Bit 10 */
| (0U << 11U)/* Bit 11 */
| (0U << 12U)/* Bit 12 */
| (0U << 13U)/* Bit 13 */
| (0U << 14U)/* Bit 14 */
| (0U << 15U)/* Bit 15 */
/** - interrupt level */
gioREG->LVLSET = 0U /* Bit 0 */
| (0U << 1U) //* Bit 1 */
| (0U << 2U) /* Bit 2 */
| (0U << 3U) /* Bit 3 */
| (0U << 4U) /* Bit 4 */
| (0U << 5U) /* Bit 5 */
| (0U << 6U) /* Bit 6 */
| (0U << 7U) /* Bit 7 */
| (0U << 8U) /* Bit 8 */
| (0U << 9U) /* Bit 9 */
| (0U << 10U)/* Bit 10 */
| (0U << 11U)/* Bit 11 */
| (0U << 12U)/* Bit 12 */
| (0U << 13U)/* Bit 13 */
| (0U << 14U)/* Bit 14 */
| (0U << 15U)/* Bit 15 */
/** - clear all pending interrupts */
gioREG->FLG = 0xFFU;
/** - enable interrupts */
gioREG->INTENASET = 0U /* Bit 0 */
| (0U << 1U) /* Bit 1 */
| (0U << 2U) /* Bit 2 */
| (0U << 3U) /* Bit 3 */
| (0U << 4U) /* Bit 4 */
| (1U << 5U) /* Bit 5 */
| (0U << 6U) /* Bit 6 */
| (0U << 7U) /* Bit 7 */
| (0U << 8U) /* Bit 8 */
| (0U << 9U) /* Bit 9 */
| (0U << 10U)/* Bit 10 */
| (0U << 11U)/* Bit 11 */
| (0U << 12U)/* Bit 12 */
| (0U << 13U)/* Bit 13 */
| (0U << 14U)/* Bit 14 */
| (0U << 15U)/* Bit 15 */
/* USER CODE BEGIN (4) */
/* USER CODE END */
}
uint32 keybufferL;
...........
void main (void)
{
/* USER CODE BEGIN (3) */
/* user_ initialization */
rtiInit();
gioInit();
.........
keybufferL = 0;
/*user main loop*/
while(1)
{
......
keybufferL = gioGetPort(gioPORTB);
......
}
/* USER CODE END */
}
Thanks,
B.Rs,
Chuan