Other Parts Discussed in Thread: TM4C129EKCPDT
Hi Guys,
I just got my Tiva Launchpad to evaluate the MCU for a security project. For that I need a unique number on each silicon.
From the datasheet (page 522), there seems to exist a set of registers for that: UNIQUEID0..3. From the datasheet:
"These registers contain a unique 128-bit identifier that cannot be modified by the user. This value is unique to each individual die but is not a random value. This unique device identifier can be used to initiate secure boot processes or as a serial number for USB or other end applications."
Seems perfect for what I want, but when I try to search for these registers while debugging, they are not there.
It's weird, because the register defined on the datasheet's previous page (PREMAC) is the last one in the SYSCTL register area.