Other Parts Discussed in Thread: TM4C129XNCZAD, SYSBIOS
Hello,
iam using CCSV6 and TivaWare_C_Series-2.1.0.12573.when i tried to shift my application address to start from address 0x00004000 instead of 0x00000000
and my MPB.cmd file :
/*
* ========MPB.cmd ========
* Define the memory block start/length for the TM4C129XNCZAD
*/
/* The starting address of the application. Normally the interrupt vectors */
/* must be located at the beginning of the application. */
#define APP_BASE 0x00004000
MEMORY
{
FLASH (RX) : origin = APP_BASE, length = 0x000fc000
SRAM (RWX) : origin = 0x20000000, length = 0x00040000
ESRAM_PART1(RWX) : origin = 0x60000000, length = 0x00100000 /* 1MB will be reserved for the FW update */
ESRAM_PART2(RWX) : origin = 0x60100000, length = 0x00700000
}
/* The following command line options are set as part of the CCS project. */
/* If you are building using the command line, or for some reason want to */
/* define them here, you can uncomment and modify these lines as needed. */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone. */
/* */
/* --heap_size=0 */
/* --stack_size=256 */
/* --library=rtsv7M4_T_le_eabi.lib */
/* Section allocation in memory */
SECTIONS
{
.intvecs: > APP_BASE
.text : > FLASH
.const : > FLASH
.cinit : > FLASH
.pinit : > FLASH
.init_array : > FLASH
.vtable : > 0x20000000
.data : > SRAM
.bss : > SRAM
.sysmem : > SRAM
.stack : > SRAM
.no_init_ram_sect : {} type=NOINIT > 0x2003c800 /* made for the loggers*/
.xram2 : {} type=NOINIT > ESRAM_PART2 /* made for the firmware update */
.xram1 : {} type=NOINIT > ESRAM_PART1
}
__STACK_TOP = __stack + 512;
i got the following error DEFAULT memory range overlaps existing memory range ,by inspection the console it was as follow
'Building target: MPB.out'
'Invoking: ARM Linker'
'Flags: -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me -g --gcc --define=PART_TM4C129XNCZAD --define=ccs --define=TIVAWARE --define=ccs="ccs" --display_error_number --diag_warning=225 --diag_wrap=off --gen_func_subsections=on -z -m"MPB.map" --heap_size=0 --stack_size=512 -i"c:/ti/ccsv6/tools/compiler/arm_5.1.9/lib" -i"c:/ti/ccsv6/tools/compiler/arm_5.1.9/include" --reread_libs --warn_sections --display_error_number --diag_wrap=off --xml_link_info="MPB_linkInfo.xml" --rom_model'
"c:/ti/ccsv6/tools/compiler/arm_5.1.9/bin/armcl" -@"ccsLinker.opt" -o "MPB.out"
<Linking>
"./configPkg/linker.cmd", line 181: warning #10096-D: specified address lies outside memory map
error #10264: DEFAULT memory range overlaps existing memory range FLASH
error #10264: DEFAULT memory range overlaps existing memory range SRAM
error #10264: DEFAULT memory range overlaps existing memory range ESRAM_PART1
error #10264: DEFAULT memory range overlaps existing memory range ESRAM_PART2
error #10010: errors encountered during linking; "MPB.out" not built
>> Compilation failure
gmake: *** [MPB.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
The linker.cmd file is created automatically each buil in ./debug/configpackgs .
Thank you
Regards
Ahmed