Other Parts Discussed in Thread: HALCOGEN
I followed the HALCoGen 04.03.00 exampe example_etpwmPulseGeneration.c for the RM46x.
The compilation in CCS 6.0.1 failed, seemingly for differences between the source example file and the etPWM API (as generated by HALCoGen into file etpwm.h.
Here are the changes I had to make to the code to make it compile (haven't checked that it runs fine yet) :
replaced ETPWM_HspClkDiv_t etpwmHspClkDiv_t ETPWM_HspClkDiv_by_1 HspClkDiv_by_1 ETPWM_ClkDiv_t etpwmClkDiv_t ETPWM_ClkDiv_by_1 ClkDiv_by_1 ETPWM_ActionQual_t etpwmActionQual_t ETPWM_ActionQual_Set ActionQual_Set ETPWM_ActionQual_Clear ActionQual_Clear ETPWM_CounterMode_t etpwmCounterMode_t ETPWM_CounterMode_Up CounterMode_Up ETPWM_setHighSpeedClkDiv() and ETPWM_setClkDiv() needed to be combined both to etpwmSetClkDiv() ETPWM_setPeriod() etpwmSetTimebasePeriod() ETPWM_setCounterMode() etpwmSetCounterMode() ETPWM_write_CmpA() etpwmSetCmpA() ETPWM_write_CmpB() etpwmSetCmpB() ETPWM_setActionQual_Zero_PwmA() etpwmSetActionQualPwmA() ETPWM_setActionQual_Zero_PwmB() etpwmSetActionQualPwmA() ETPWM_setActionQual_CntUp_CmpA_PwmA() etpwmSetActionQualPwmA() ETPWM_setActionQual_CntUp_CmpB_PwmB() etpwmSetActionQualPwmB() ETPWM_setCount() etpwmSetCount()
Here is the list of compilation/link errors I had with the original code.
"../source/sys_main.c", line 62: error #20: identifier "ETPWM_HspClkDiv_t" is undefined "../source/sys_main.c", line 62: error #20: identifier "ETPWM_HspClkDiv_by_1" is undefined "../source/sys_main.c", line 63: error #20: identifier "ETPWM_ClkDiv_t" is undefined "../source/sys_main.c", line 63: error #20: identifier "ETPWM_ClkDiv_by_1" is undefined "../source/sys_main.c", line 67: error #20: identifier "ETPWM_ActionQual_t" is undefined "../source/sys_main.c", line 67: error #20: identifier "ETPWM_ActionQual_Set" is undefined "../source/sys_main.c", line 68: error #20: identifier "ETPWM_ActionQual_t" is undefined "../source/sys_main.c", line 69: error #20: identifier "ETPWM_ActionQual_t" is undefined "../source/sys_main.c", line 69: error #20: identifier "ETPWM_ActionQual_Clear" is undefined "../source/sys_main.c", line 70: error #20: identifier "ETPWM_ActionQual_t" is undefined "../source/sys_main.c", line 71: error #20: identifier "ETPWM_CounterMode_t" is undefined "../source/sys_main.c", line 71: error #20: identifier "ETPWM_CounterMode_Up" is undefined "../source/sys_main.c", line 75: warning #225-D: function "ETPWM_setHighSpeedClkDiv" declared implicitly "../source/sys_main.c", line 78: warning #225-D: function "ETPWM_setClkDiv" declared implicitly "../source/sys_main.c", line 81: warning #225-D: function "ETPWM_setPeriod" declared implicitly "../source/sys_main.c", line 84: warning #225-D: function "ETPWM_setCounterMode" declared implicitly "../source/sys_main.c", line 87: warning #225-D: function "ETPWM_write_CmpA" declared implicitly "../source/sys_main.c", line 90: warning #225-D: function "ETPWM_write_CmpB" declared implicitly "../source/sys_main.c", line 93: warning #225-D: function "ETPWM_setActionQual_Zero_PwmA" declared implicitly "../source/sys_main.c", line 96: warning #225-D: function "ETPWM_setActionQual_Zero_PwmB" declared implicitly "../source/sys_main.c", line 99: warning #225-D: function "ETPWM_setActionQual_CntUp_CmpA_PwmA" declared implicitly "../source/sys_main.c", line 102: warning #225-D: function "ETPWM_setActionQual_CntUp_CmpB_PwmB" declared implicitly "../source/sys_main.c", line 105: warning #225-D: function "ETPWM_setCount" declared implicitly 12 errors detected in the compilation of "../source/sys_main.c". undefined first referenced symbol in file --------- ---------------- ETPWM_setActionQual_CntUp_CmpA_PwmA ./source/sys_main.obj ETPWM_setActionQual_CntUp_CmpB_PwmB ./source/sys_main.obj ETPWM_setActionQual_Zero_PwmA ./source/sys_main.obj ETPWM_setActionQual_Zero_PwmB ./source/sys_main.obj ETPWM_setClkDiv ./source/sys_main.obj ETPWM_setCount ./source/sys_main.obj ETPWM_setCounterMode ./source/sys_main.obj ETPWM_setHighSpeedClkDiv ./source/sys_main.obj ETPWM_setPeriod ./source/sys_main.obj ETPWM_write_CmpA ./source/sys_main.obj ETPWM_write_CmpB ./source/sys_main.obj
Here is the resulting source file:
void main(void)
{
/* USER CODE BEGIN (3) */
// ETPWM_HspClkDiv_t hsClkDiv=ETPWM_HspClkDiv_by_1;
etpwmHspClkDiv_t hsClkDiv=HspClkDiv_by_1;
// ETPWM_ClkDiv_t clkDiv=ETPWM_ClkDiv_by_1;
etpwmClkDiv_t clkDiv=ClkDiv_by_1;
uint16 period=0x24;
uint16 pwmData1=period/2;
uint16 pwmData2=period/4;
// ETPWM_ActionQual_t actionQual1= ETPWM_ActionQual_Set;
etpwmActionQual_t actionQual1= ActionQual_Set;
// ETPWM_ActionQual_t actionQual2= ETPWM_ActionQual_Set;
etpwmActionQual_t actionQual2= ActionQual_Set;
// ETPWM_ActionQual_t actionQual3= ETPWM_ActionQual_Clear;
etpwmActionQual_t actionQual3= ActionQual_Clear;
// ETPWM_ActionQual_t actionQual4= ETPWM_ActionQual_Clear;
etpwmActionQual_t actionQual4= ActionQual_Clear;
// ETPWM_CounterMode_t counterMode=ETPWM_CounterMode_Up;
etpwmCounterMode_t counterMode=CounterMode_Up;
uint16 count=0;
/* set the high speed clock divider */
// ETPWM_setHighSpeedClkDiv(etpwmREG1,hsClkDiv);
/* set the normal clock divider */
// ETPWM_setClkDiv(etpwmREG1,clkDiv);
/* needed to combine previous two calls into one call */
etpwmSetClkDiv(etpwmREG1, clkDiv, hsClkDiv);
/* set the period of pwm */
// ETPWM_setPeriod(etpwmREG1,period);
etpwmSetTimebasePeriod(etpwmREG1,period);
/* set the counter direction-up,down or updown */
// ETPWM_setCounterMode(etpwmREG1,counterMode);
etpwmSetCounterMode(etpwmREG1,counterMode);
/* set the compare register CMPA to adjust the duty cycle for ETPWM1A pin */
// ETPWM_write_CmpA(etpwmREG1,pwmData1);
etpwmSetCmpA(etpwmREG1,pwmData1);
/* set the compare register CMPB to adjust the duty cycle for ETPWM2A pin */
// ETPWM_write_CmpB(etpwmREG1,pwmData2);
etpwmSetCmpB(etpwmREG1,pwmData2);
/* set the action qualifier for the generation of events at counter equals 0 for ETPWM1A */
// ETPWM_setActionQual_Zero_PwmA(etpwmREG1,actionQual1);
etpwmSetActionQualPwmA(etpwmREG1,actionQual1);
/* set the action qualifier for the generation of events at counter equals 0 for ETPWM1B */
// ETPWM_setActionQual_Zero_PwmB(etpwmREG1, actionQual2);
etpwmSetActionQualPwmA(etpwmREG1, actionQual2);
/* set the action qualifier for the generation of events at counter equals compare value of A for ETPWM1A */
// ETPWM_setActionQual_CntUp_CmpA_PwmA(etpwmREG1, actionQual3);
etpwmSetActionQualPwmA(etpwmREG1, actionQual3);
/* set the action qualifier for the generation of events at counter equals compare value of B for ETPWM1B */
// ETPWM_setActionQual_CntUp_CmpB_PwmB(etpwmREG1, actionQual4);
etpwmSetActionQualPwmA(etpwmREG1, actionQual4);
/* set and initialize the counter */
// ETPWM_setCount(etpwmREG1,count);
etpwmSetCount(etpwmREG1,count);
/* ... run forever */
while(1);
/* USER CODE END */
}