Other Parts Discussed in Thread: RM57L843, TMS570LC4357, TMDS570LS31HDK
TMDXRM57LHDK Schematics, page 10 of 29 Rev. B, shows a few connections that seem not not match RM57L843 or TMS570LC4357 datasheets. (The schematics do match the actual pcb layout though).
Datasheets Indicate:
J14 - Core Logic Voltage 1.2V
V19 - AD2IN[24] Input
W18 - AD2IN[24] Input (Alternate)
Schematic Indicates:
J14 - VCCPLL2
V19 - VSSAD (grounded)
W18 - VSSAD (grounded)
Q1: Is there a clarification regarding J14, should be used as VCCPLL2?
Q2: Are V19 and W18 actually VSSAD ground, or are they grounded for A2D ground conversion reference?
Q3: Are the micros RM57L843 and TMS570LC4357 pin compatible regarding Power and etc? (Other than feature differences)
Thanks :)