I just ran into this issue using:
CCSV6.1.0 (most recent update)
TI-RTOS (most recent update 2.10.01.38)
XDC Tools (3.31.00.24)
Target is T4MC1233H6PM
SmartRF06 board jumpered to T4MC1233H6PM JTAG pins as XDS100v3.
Running Windows 7 on Xenon E31230
Screen capture and comment in attached pdf (picture is worth 1000 words).
.I've seen references to this popping up in other posts with no real good explanation as to how it happens and how to avoid it. Admittedly, there is a 4 inch of ribbon between the SmartRF06 board and the target (the board is custom design).
The application is incredibly simple, packets fed in on UART0, buffered then transmitted out on UART1. When I jumper the source and target together without involving the Tiva Chip, it works as intended. I've been an engineer for 38 years, this is the first time I've had this much "adventure" developing something as simple as this.
This is only one in a long series of "issues" that keep cropping up with what should be a straightforward tool-chain. Is there a possible incompatibility running your tool-chain (CCSV6) on the Xenon processor (just a desperate grasp at an explanation).