dear e2e ,
We are working on tms570ls3137 processor for one of our project , ide we are using is ccs v 6.0 , also halcogen v 4.4.0 for configuration
We are trying to communicate with FLASH IC( IS25CQ032 ) using SPI communication .
We have enabled SPI2 and N2HET1 in halcogen , where N2HET1 which are used as GPIO for chip select of SPI . We have configured TMS as master and flash as slave with the baud rate 8MHZ. and 8 bit charter length.
We are doing successive flash write and read data from the flash in tight loop . i have attached file which contains the function which i am using., Here by using this i am writing into the flash one sector followed by another Writing in to the flash (not same sector )and reading the flash , When we are doing successive flash write, if we give the delay b/w successive flash write in the code , I am able to write data into flash correctly. if i tired write to flash without giving delay b/w two successive flash write it's not writing data into flash memory. can you tell the reason4478.flah_function.docx for this.
Thank You.