This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DK-TM4C129X User's Manual - Errata/Update - Pin listing inconsistent between document and schematic

I need to connect all pins of  J6,J9, J27,J28,J29, J30 and J34 to external board, but checking the pinout on the schematics and the documentation shows totally different things. 

For example, J9-3 is written as PQ0 on the table at page 12, but in page 4 of the schematic (Pg 32),  this pin is connected to PJ3. 
And one more - J6-10 is written as PT0 on the table, but shown as PB5 on the schematic.

Attached are prints of the two pages, with marking.

Note that I'm using the User's Guide linked in the DX's page: http://www.ti.com/lit/pdf/spmu360  - SPMU360 Dated October 2013.

In some trials I've found that the schematic is correct.  

Is there an update to the User's Manual?

Can I get at least the updated tables?

Document0.pdf

Pin# Board Location
V3 #N/A
W3 #N/A
U5 #N/A
V4 #N/A
W4 #N/A
V5 #N/A
R7 #N/A
A16 #N/A
B16 #N/A
A17 #N/A
B17 #N/A
B6 #N/A
F2 #N/A
F1 #N/A
B15 #N/A
C15 #N/A
D14 #N/A
C14 #N/A
M2 #N/A
M1 #N/A
L2 #N/A
K3 #N/A
D2 #N/A
A4 #N/A
B4 #N/A
B3 #N/A
B2 #N/A
A5 #N/A
B5 #N/A
B7 #N/A
U6 #N/A
V6 #N/A
V7 #N/A
W7 #N/A
T8 #N/A
U8 #N/A
N15 #N/A
T14 #N/A
M16 #N/A
V12 #N/A
P4 #N/A
R2 #N/A
R1 #N/A
T1 #N/A
R3 #N/A
T2 #N/A
C8 #N/A
E7 #N/A
F16 #N/A
F18 #N/A
E17 #N/A
N1 #N/A
V16 #N/A
W16 #N/A
G16 #N/A
H19 #N/A
G18 #N/A
J18 #N/A
C18 #N/A
B18 #N/A
K18 #N/A
K19 #N/A
L18 #N/A
L19 #N/A
B10 #N/A
A10 #N/A
B9 #N/A
T12 #N/A
D7 #N/A
B13 #N/A
C12 #N/A
D8 #N/A
B12 #N/A
B8 #N/A
A8 #N/A
A13 #N/A
N5 #N/A
N4 #N/A
N2 #N/A
V8 #N/A
P3 #N/A
P2 #N/A
W9 #N/A
R10 #N/A
V9 #N/A
T13 #N/A
V10 #N/A
E18 #N/A
F17 #N/A
V2 U5TX
U2 U5RX
M4 T7CCP1
N18 T5CCP1
G15 T4CCP1
A14 T3CCP1
B14 T3CCP0
D13 T2CCP1
D12 T2CCP0
D1 T1CCP1
G19 T0CCP1
C1 T0CCP0
H18 T0CCP0
T7 SSI3CLK
U14 SSI2CLK
T6 SSI0CLK
K17 SPI_B_SOMI
K15 SPI_B_SIMO
H4 PQ2
E2 PQ1
U12 PN7
E3 INT. GPIO
M3 INT. GPIO
C6 GPIO
H17 GPIO
K5 GPIO
C10 GPIO
B11 GPIO
A11 GPIO
U10 GPIO
R13 GPIO
W10 GPIO
V11 EN0TXCLK
U19 EN0RXD3/EPI0S32/EN0LED0
V17 EN0RXD2/EPI0S31/EN0LED2
U15 EN0RXD1
W12 EN0RXD0
M18 EN0RREFCLK
W6 EN0MDC
D6 EN0INTRN
N19 EN0CRS
A7 AIN20
K2 AIN19
K1 AIN18
J2 AIN17
J1 AIN16
C2 AIN15
H3 AIN03
H2 AIN02
G1 AIN01
G2 AIN00