Hallo!
Knowing that it should be possible (because Energie is doing it) I tried to compile some c++ files for my project. (Actually this was my 4th try but now...) everyting worked fine and I got some running code. So I startet to port over my complete project which was until now only simulating OOP in C.
Two days later I got stuck with this problem which I tried to solve with the help of Stackoverflow: https://stackoverflow.com/questions/37194071/c-global-object-initialization-fails-why-and-is-it-possible-to-put-objects/37194313
It seems that this isn't a problem with my understanding of C++ but imho a problem with the default startup_gcc/linker code which I've taken from some example project and which won't work completely for c++.
So I guess my question is: where do I get startup_gcc and ld files which will work with c++ code?
Thanks & best regards,
Florian