Other Parts Discussed in Thread: UNIFLASH, HALCOGEN, RM57L843
Chip: RM48L952ZWT
Environment: Halcogen, CCS (Code Composer Studio), UniFlash, TI compiler
Memory: 16MB SDRAM plus internal to the chip; stack uses internal, while heap uses the external
How can I determine how much of the stack and memory I am using and if I am getting close to filling or exceeding one of the sections?
MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH0 (RX) : origin=0x00000020 length=0x0017FFE0
FLASH1 (RX) : origin=0x00180000 length=0x00180000
STACKS (RW) : origin=0x08000000 length=0x0003fe00
RAM (RW) : origin=0x0803fe00 length=0x00000200
/* USER CODE BEGIN (2) */
RAM2 (RW) : origin=0x80000000 length=0x01000000
/* USER CODE END */
}
SECTIONS
{
.intvecs : {} > VECTORS
.text : {} > FLASH0 | FLASH1
.const : {} > FLASH0 | FLASH1
.cinit : {} > FLASH0 | FLASH1
.pinit : {} > FLASH0 | FLASH1
.bss : {} > RAM2
.data : {} > RAM2
.sysmem : {} > RAM2
FEE_TEXT_SECTION : {} > FLASH0 | FLASH1
FEE_CONST_SECTION : {} > FLASH0 | FLASH1
FEE_DATA_SECTION : {} > RAM2
#endif
/* USER CODE END */
}