Other Parts Discussed in Thread: EK-TM4C123GXL
Hello,
About 1 month ago i ask your help for initializing an round display for a smartwatch.
Now i am trying to make the touchscreen work but i had no luck.
Its datasheet is not very explicit. I am using I2C for it, but i have some questions:
Its address is : 1000100, with a R/W bit, R=0,W=1 and 8 bits after that should be the read value.
I will attach the datasheet.
My code is a little bit complex (got over 2500 lines) so it doesn t make sense to post it all.
My touchscreen is connected to PB2 and PB3. So its I2C0 module.
#define SLAVE_ADDRESS 0x8C
void I2C_Init()
{
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB); //Enable GPIOB// this line is not actually here, its in the main
ROM_SysCtlPeripheralEnable (SYSCTL_PERIPH_I2C0);
GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2);
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_3);
GPIOPinConfigure (GPIO_PB2_I2C0SCL);
GPIOPinConfigure (GPIO_PB3_I2C0SDA);
I2CMasterInitExpClk(I2C0_BASE, SysCtlClockGet(), false); //DE CE TRUW!?!?!?
I2CMasterEnable (I2C0_BASE);
}
uint32_t I2CReceive(uint32_t slave_addr, uint8_t reg)
{
//specify that we are writing (a register address) to the
//slave device
I2CMasterSlaveAddrSet(I2C0_BASE, slave_addr, false);
//specify register to be read
I2CMasterDataPut(I2C0_BASE, reg);
//send control byte and register address byte to slave device
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_SINGLE_SEND);
//wait for MCU to finish transaction
while(I2CMasterBusy(I2C0_BASE));
//specify that we are going to read from slave device
I2CMasterSlaveAddrSet(I2C0_BASE, slave_addr, true);
//send control byte and read from the register we
//specified
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_SINGLE_RECEIVE);
//wait for MCU to finish transaction
while(I2CMasterBusy(I2C0_BASE));
//return data pulled from the specified register
return I2CMasterDataGet(I2C0_BASE);
}
This function I2CReceive(SLAVE_ADDRESS,reg); returns always the same value no matter where i touch the CTP (Capacitive Touchscreen Panel). Can anyone help me? Some ideas?
Thank you! I don t have an oscilloscope right now so i can view the signals.